Skip to Main Content
  • English
  • 简体中文
  • 繁體中文
Contact
View Cart
Automotive application of Wolfspeed power products in an electric vehicle on the road
Applications

Automotive

Wolfspeed’s Silicon Carbide semiconductors are putting EV systems designers in the driver’s seat.

Unlock A New Era of EV Efficiency with Wolfspeed Silicon Carbide.

Silicon Carbide (SiC) technology can positively influence every major power path of an EV system. EVs utilizing Wolfspeed Silicon Carbide products have a lower overall system cost, and the ability to realize a more reliable operation in every section of the vehicle. Explore how Silicon Carbide is driving the EV revolution.


Wolfspeed's 6.6 kW High Power Density Bi-Directional EV On-Board Charger Reference Design.
Wolfspeed's 6.6 kW High Power Density Bi-Directional EV On-Board Charger Reference Design.

A Market in Motion

Wolfspeed launched the industry’s first Silicon Carbide (SiC) MOSFET in 2011 and has been leading the transformation from silicon to Silicon Carbide in EVs ever since. No longer constrained by the limitations of Si devices, EV designers embraced the faster switching speeds and greater power density that only Silicon Carbide MOSFETs and Schottky diodes enable, building smaller, lighter, and more efficient motors. Reducing power losses by nearly 80% also reduces consumers’ “range anxiety” by extending driving distance by up to 10%.

Wolfspeed offers the industry’s most comprehensive portfolio of high-performance, high-capability Silicon Carbide components, including our automotive-grade E-Series, a family of ruggedized devices which are the first commercially available Silicon Carbide MOSFETs and diodes to be AEC-Q101 automotive qualified and PPAP capable. The E-Series offers designers the highest available power density and can handle the harshest environments for both on-board and off-board automotive power conversion systems.


Automotive Applications

Wolfspeed SiC Power for EV Powertrain / Main Inverter

EV Powertrain / Main Inverter

All EV powertrains propel their host vehicle, but exactly how that’s accomplished is up to the designer. He or she seeks to devise an elegant system which fluidly induces all the moving parts to do their jobs faster, using less power, at a lower price point. Many are designing around Wolfspeed’s 1200V Silicon Carbide MOSFET for its capability to handle high current with the industry’s lowest drain-source on resistance, which increases the distance consumers can drive on a single charge.

Learn More

Car with transparent backgroundFast Charging SystemsOn-Board Charging SystemsPowertrain SystemsOn-Board DC/DC Converter

Knowledge Center

View All
Fast Charging

Maximize Efficiency in Isolated DC/DC Converters for EV Fast Charging Systems

Designing with Silicon Carbide (SiC) for Electric Vehicle DC Fast Chargers.
Continue Reading  White Paper
Technical SupportPower Applications Forum

Footer

Social Media

  • Instagram
  • X
  • LinkedIn
  • YouTube
Copyright © 2025 Wolfspeed, Inc.