Silicon Carbide Manufacturing Leadership
Increasing capacity to address steepening demand
Five Investments Bolstering Our Industry-Leading Manufacturing Position
We have $6.5B in CapEx committed through 2027 for:
- Expanding our existing Durham, NC materials facility
- Building the “The John Palmour Manufacturing Center for Silicon Carbide” in Siler City, NC
- Ramping the world’s first 200 mm Silicon Carbide fab in Mohawk Valley (Marcy, NY)
- A planned second 200 mm fab in Saarland, Germany
- Establishing multi-site epitaxy footprint with purchase of Farmers Branch, TX epi facility
World's 1st
commercially available, fully qualified silicon carbide MOSFET
SiC Leadership
Wolfspeed is the leader in silicon carbide technology
13+ trillion
silicon carbide device field hours
The John Palmour Manufacturing Center: Increasing Wolfspeed Materials Capacity by 10x
This state-of-the-art Silicon Carbide wafer facility will:
- Focus on 200 mm wafers
- Span 1.8 km2 (445 acres)
- Be highly-automated
- Create 1,800 new jobs by 2030
- Cover more than 185,806 m2 (2 million ft2)
Mohawk Valley Fab: Ramping Production and Qualifications Now
First and largest 200 mm Silicon Carbide Power Fab:
- Will be 20% utilized by July 2024; ramps continue through 2027
- Fully automated lights-out fab
- Automotive quality systems designed-in
- IATF certified on first pass
- Site spans 220,000 m2 (55 acres)
- Cover more than 46,451 m2 (484,000 ft2)
- Building is more than 46,451 m2 (484,000 ft)2
- LEED Silver certified energy efficient building
Plans to Construct European Device Fab Starting in 2024
Will be Wolfspeed’s largest and most advanced 200 mm SiC fab
- Located in Saarland, Germany
- Estimated at >$2 billion investment
- Optimized for innovative manufacturing processes
- Planned to build next generation Silicon Carbide devices
- Designed to be a model for fab sustainability
- Contingent upon IPCEI funding approvals
Recent Purchase of Epitaxy Facility in Farmers Branch, Texas
Extending our epitaxy capacity:
- Establishes multi-site epi footprint
- Automated tools
- Initial ramp beginning in middle of 2024
- Spans 0.6 km2 (16.28 acres)
- Site covers more than 26,000 m2 (280,000 ft2)
- Will support 150 mm and 200 mm wafers
Diversifying our Global Footprint with Multisite Expansion
Materials and/or epi site
Fabrication site
Packing and TDI site
*Purple text denotes existing footprint
*Teal text denotes future footprint