Wolfspeed Logo

Main menu navigation

  • Explore Products

    • Power Modules
    • Discrete MOSFETs
    • Discrete Schottky Diodes
    • Bare Die MOSFETs
    • Bare Die Schottky Diodes
    • Reference Designs
    • Gate Driver Boards
    • Evaluation Kits
    • Materials Products
  • Explore Applications

    • Artificial Intelligence

      • Datacenter & Server Power Supplies
      • Uninterruptible Power Supplies
    • Automotive

      • EV Powertrain
      • On-Board Charger
      • On-Board DC/DC Converter
    • E-Mobility

      • Commercial, Construction & Agriculture Vehicles
      • E-Boats and E-Ships
      • Trains & Traction
    • Industrial Motor Drives

      • Low Voltage Motor Drives
      • Heat Pump & Air Conditioning
      • Servo Drives
    • Renewable Energy

      • Energy Storage Systems
      • Fast Charging
      • Residential & Light Commercial Solar Systems
      • Industrial & Commercial Solar Systems
      • Utility Scale Renewable Energy
    • Materials Applications
  • Tools & Support
  • Explore Company

    • About
    • Locations
    • Senior Leadership
    • Thought Leadership
    • Quality
    • Sustainability
    • News
    • Events
  • Careers
  • Investors
  • English
  • 简体中文 - Chinese (Simplified)
  • 繁體中文 - Chinese (Traditional)
Contact
    View Cart

    Breadcrumb Navigation

    • Home
    • Knowledge Center
    • Heat Pumps & Air Conditioning
    • Beat the Heat This Summer with Wolfspeed SiC in Residential & Commercial Air Conditioners and Heat Pumps 
    Heat Pumps & Air Conditioning

    Beat the Heat This Summer with Wolfspeed SiC in Residential & Commercial Air Conditioners and Heat Pumps 

    Sep 05, 2024
    • Share on LinkedIn
    • Share on Facebook
    • Share on Twitter
    • Share in an email

    Article

    Introduction 

    Silicon carbide is revolutionizing the heat pump and air conditioning industry by delivering unprecedented efficiency, enhanced durability, and superior performance in the most challenging of environments. Increasing global temperatures necessitate stricter efficiency regulations, which SiC powered solutions can achieve with either minimal retrofitting of existing designs or completely new system designs. This article will guide you through the technical considerations and practical applications of SiC discrete solutions and power modules in both residential and commercial heat pump and air conditioner designs.  

    Increasing efficiency standards driving system evolution 

    In the United States, the efficiency of heating and cooling systems is measured based on a national standard called the Seasonal Energy Efficiency Ratio (SEER). Beginning in 2023, all new residential central air conditioning and air source heat pump systems sold in the United States were required a SEER (Seasonal Energy Efficiency Ratio) rating of no less than 14 in the northern states and 15 SEER in the southern states, where cooling consumes a larger share of home energy use.  

    Similar standards exist in Europe called ESEER (European Energy Efficiency Ratio) that push new systems to be rated B or above to stay competitive in an energy conscious market. China has GB21455 Efficiency Standards pushing new designs to aim for higher efficiency grades but no lower than 5. 

    Heat pump and air conditioning standards from America, Europe, and China.
    Figure 1: Heat pump and air conditioning efficiency standards are measured across the globe based on varying standards.  

    Figure 1 illustrates the increasingly strict standards in the U.S., Europe and China. Meeting these requirements is difficult for legacy power semiconductor devices. Silicon carbide provides a simple, cost-effective way to meet these standards while enabling smaller, more power dense and quieter overall heating and cooling systems.  

    A collection of labeled circuit diagrams that show what subsystems make up heat pumps and air conditioners. Some areas are highlighted, to show the correct PFC and Inverter to use.
    Figure 2: The various subsystems comprising heat pumps and air conditioners. The highlighted areas represent the PFC and inverter used to power up the compressor motor (Source: Electronicproducts) 

    Improving efficiency with simple drop-in silicon carbide devices 

    Silicon carbide discrete devices can be easily integrated into existing heat pump and air conditioner designs enabling sufficient gains in efficiency to meet SEER, ESEER and GB21455 standards. Figure 2 illustrates the various subsystems of heat pumps and air conditioners including power conversion (PFC) and inverters, which together work to power the compressor and provide desired air temperature. 

    Two block diagrams explaining how to upgrade a PFC to use a Silicon Carbide diode. This method can be done without a redesign.
    Figure 3: Upgrading the PFC with SiC Diode (no redesign approach)  

    Figure 3 shows the typical silicon-based PFC in an active boost configuration and how it can be easily improved by simply replacing the silicon diode with a 650 V or 1200 V (depending upon the DC bus voltage) silicon carbide (SiC) Schottky diode without any system redesign. This is a very popular upgrade and yields around 0.5% or even higher increase in efficiency. 

    Wolfspeed’s 650 V and 1200 V Schottky diodes offer zero reverse recovery charge (Qrr) when compared to silicon diodes. Wolfspeed’s C4D 1200 V and C3D 650 V SiC diode series provides the best reverse recovery performance when compared to any Si diodes in the market (Fig.4).  

    Two side by side line grades showing the Reverse Recovery losses for Wolfspeed's SiC Shottky Diodes compared to products that use Silicon
    Figure 4: Wolfspeed’s silicon carbide (SiC) Schottky diodes offer magnitudes lower reverse recovery loss

    Redesigning with SiC Realizes Further Efficiency Gains

    The performance benefits of silicon carbide can be further maximized by redesigning the PFC in a semi-bridgeless or bridgeless totem pole configuration (Fig. 5).

    Two PFC block diagrams showing a semi-bridgeless (left image) and bridgeless(right image). Both diagrams use a "totem pole" configuration.
    Fig. 5: Redesigning the PFC stage in a semi-bridgeless (left) and bridgeless (right) totem pole configuration

    Implementing a semi-bridgeless PFC topology by using two SiC 650/750 V MOSFETs on the fast-switching leg along with two SiC 650/1200 V diodes for the slow switching leg (depending upon DC link voltage) can improve the system efficiency by 1.5% over a silicon-based boost PFC.

    Similarly, a full bridgeless PFC topology using all SiC MOSFETs on both the fast and slow switching leg can improve system efficiency by 1.9% over Si based boost PFC. For reference, in a 11 kW compressor system switching at 16 kHz (Fig. 6), the total losses of the system can be reduced more than 50% when using SiC compared to a Silicon-based solution.

    Two side by side bar graphs showing motor driver losses between a Silicon MOSFET (left) and a Wolfspeed Silicon Carbide MOSFET (right). Both graphs are shown with the products in an 11 kW, 16 kHz system operating at 50% load.
    Figure 6: motor driver losses for Si d vs. Silicon carbide 650 V MOSFETs in an 11 kW, 16 kHz system operating at 50% load 
    Line graph showing how Wolfspeed's SiC MOSFETs translates to big gains in reduced shipping losess.
    Figure 7: Wolfspeed’s SiC MOSFETs smallest Qrr translates to big gains in reduced switching losses 

    Silicon MOSFETs are not well suited to bridgeless PFC topologies due to their large reverse recovery (Fig. 7), and silicon IGBTs exhibit high switching losses, requiring lower switching frequencies and larger magnetic components resulting in a more costly solution. 

    Thanks to an improved switching performance and better thermals, this redesign approach reduces the audible noise and easily transitions new industrial motors installations from (International Efficiency) IE3 to IE4 and IE5 regulation as per IEC60034-14 standard (Fig 8). 

    Line chart showing IEC standards for Industrial Motor Drives
    Figure 8: IEC standards for Industrial Motor Drives 

    Additional gains in the inverter stage redesign  

    The inverter stage comprising of 6 switches can be easily upgraded into a full SiC solution by replacing all the existing IGBT switches (Fig. 9).  

    A block diagram showing what it would look like if an inverter used SiC switches instead of IGBT switches.
    Figure 9: Replacing IGBT switches with SiC switches in the inverter stage 

    Wolfspeed’s SiC MOSFETs deliver the lowest conduction losses when compared to typical IGBT solutions. The figure below illustrates conduction losses for a 1200 V Wolfspeed SiC MOSFET vs a legacy IGBT. At a low load SiC MOSFETs deliver a 50% reduction in losses at a 30% load and  30% reduction in conduction losses at a half load (Fig. 10).  

    Line graph showing the conduction losses for Wolfspeed's 1200 V, 40 A, Silicon Carbied MOSFET versus a comparable IGBT
    Figure 10: Conduction losses for Wolfspeed’s 1200 V 40 A SiC MOSFET vs a comparable IGBT

    When a 1200 V SiC MOSFET’s switching is compared with a typical 1200 V IGBT, the advantage of ultra-low switching loss is evident as there is no trail current visible during turn off. This feature of a SiC MOSFET in turn provides up to 95% lower turn off switching losses or 85% overall total switching losses (Fig. 11).

    A shaded line graph showing the IGBT's tail current impacts the turn-off loss (right) versus the tail current being with 1200 V Silicon Carbide MOSFET
    Figure 11: The IGBT tail current impacts the turn-off loss (right) vs the tail current being eliminated with 1200 V SiC MOSFET. 

    Additional savings with reduced Heatsink 

    In addition to consuming less power, SiC enables smaller and less expensive cooling designs in heat pumps and air conditioners due to improved thermal performance. For a 25 kW inverter operating at 8 kHz, using Wolfspeed’s 6 switch WolfPACK® module compared to a similar IGBT modules leads to an overall 77% size reduction in the heatsink (Fig. 13) along with 1.1% improved efficiency. This is on inverter side alone, and when combined with a SiC powered Totem Pole PFC, a combined efficiency of 2.6% can be observed (Fig. 12). 

    Thermal comparison between Wolfspeed's Silicon Carbide MOSFET CCB032M12FM3 versus comparable Silicon IGBTs
    Figure 12: Efficiency and thermal comparison between Wolfspeed’s WolfPACK® Module and an IGBT solution
    Comparison between an IGBT heat-sink and Wolfspeed's WolfPACK.
    Figure 13: Heatsink size comparison between Wolfspeed’s WolfPACK® and an IGBT solution

    SiC based inverters provide a significant reduction in system-generated heat, enabling designers to use smaller heat sinks and design overall smaller, lighter compressors for air conditioners and heat pump systems.

    Design support tools to lower the barrier to entry with SiC

    Wolfspeed offers a suite of design support tools tailored to heat pumps and air conditioning that can help lower the barrier to entry when designing with SiC and speed your overall system optimization process.

    Wolfspeed’s recently released 11kW High Efficiency Inverter reference design (CRD-11DA12N-K) (Fig. 14) features Wolfspeed’s 75 mΩ 1200 V MOSFETs and provides a perfect platform to test the advantages of SiC in heat pump and air conditioning compressor inverters. This design is characterized for thermals, inductance and circuit operation and features a simple 2-level, 3-phase topology with customizable firmware.

    Wolfspeed Power Reference Design CRD-11DA12N-K 11 kW Motor Drive
    Figure 14: CRD-11DA12N-K

    This inverter design can easily be upgraded to 20 kW by using Wolfspeed’s 40 mΩ C3M0040120K. When compared to an IGBT solution, the SiC solution outperforms an IGBT solution by up to 1.7% efficiency gains at 16 kHZ and up to 3.5% efficiency gain at 32 kHz, even when operating at lower dv/dt values to protect the motor (Fig. 15).

    Line graph comparison between C3MK0040120K
    Figure 15: Efficiency gains realized when comparing Wolfspeed’s 40 mΩ 1200 V MOSFET to comparable IGBT solution. 

    Building upon Wolfspeed’s SpeedVal™ Kit Modular Evaluation Platform, the newly released Three-Phase Motherboard further speeds the transition from silicon to silicon carbide with a flexible set of building blocks for in-circuit evaluation of system performance. Designed with industrial motor drives, heat pumps and air conditioning systems in mind, SpeedVal Kit enables designers to rapidly evaluate and optimize silicon carbide MOSFETs paired with gate drivers from industry-leading partners. The 3-phase motherboard also enables precise control and firmware development with flexible control options to test simple static loads or advanced motor control function.  

    Savings & Environmental Impact 

    The environmental impact from upgrading heating and air conditioning systems with SiC in just the PFC and inverter is significant. For reference, with a three-phase 11 kW system, the consumer can expect to save at least 453 kWh of energy annually, or about €168 euros and more than offset any increase in system cost. These savings are especially significant when you look at the lifetime use of the unit. Assuming the system lasts 15 years, consumers will save 6800 kWh totaling around €2,520 euro. This also translates to 4.8 Metric tons of less CO2 * being released into the atmosphere, making SiC a more sustainable choice for designing next generation heat pumps and air conditioners.  

    General design recommendations for cleaner layout 

    • Designers are recommended to avoid overlapping between gate driver circuit and the drain of the MOSFET (Fig. 16a). This helps in reducing the risk of inducing external Cgd in the gate drive power loop. Benefits include:
      • Lower switching losses
      • Reduced risk of gate oscillation
      • Lower EMI
    • Keep sensitive signals away from the high dv/dt traces. Reducing the size of switching node traces minimizes parasitic capacitance to the DC bus, which reduces switching losses and EMI concerns. (Fig. 16b)
    • Minimize the gate loop for the gate driver circuit as much as possible and place the external Cgs cap as close as possible to the MOSFET.
    Figure 16: (a) Typical gate drive loop of the MOSFET; (b) Switch nodes in the inverter stage  

    *(www.epa.gov) 

    Summary 

    With the rise in global temperatures there is an ever-increasing need for greener solutions to combat climate change. As demonstrated, SiC is a more sustainable choice when designing the next generation of heat pumps and air conditioners residential, industrial and commercial applications.  

    Designing with SiC has never been easier with Wolfspeed’s 11kW High Efficiency Inverter reference design (CRD-11DA12N-K) that can be powered up to 20 kW acting as a guiding tool to unleash the power of SiC and surpass new efficiency standards with ease. You can even simulate your design challenges today with our online SpeedFit® Design Simulator, quickly prototype and test using the SpeedVal evaluation platform, or connect directly with our silicon carbide experts at our Power Applications Forum. 

    Technical SupportPower Applications Forum
    Request SamplesVisit the Sample Center
    SpeedFit Design SimulatorCreate a Design

    Support

    Technical SupportPower Applications Forum
    Request SamplesVisit the Sample Center
    SpeedFit Design SimulatorCreate a Design

    Footer

    Wolfspeed Logo

    Social Media

    • Instagram
    • X
    • LinkedIn
    • YouTube

    Footer Navigation

    • Contact
    • Where to Buy
    • Intellectual Property
    • Suppliers & Contractors

    Legal

    • Privacy Policy
    • Cookie Policy
    • Terms Of Use
    • Accessibility
    Copyright © 2026 Wolfspeed, Inc.

    More Articles

    View All

    Gen 4 Silicon Carbide Technology:
    Redefining Performance and Durability in High-Power Applications

    Continue Reading White Paper

    Two Engineers, One SpeedVal™ Kit:
    Unlock the power of silicon carbide in Industrial Motor Drives with SpeedVal Kit

    Accelerate and de-risk the silicon carbide design process for three-phase industrial motor drives and meet leading efficiency standards with the SpeedVal™ Kit Three-Phase Motherboard.
    View Now Webinars

    Practical Tools for Designing with Silicon Carbide in Industrial Motor Drives

    Simplify, accelerate and de-risk the design process when designing industrial motor drives with silicon carbide and easily access IE4 and IE5 efficiency standards.
    Continue Reading Blog