Wolfspeed Logo

Main menu navigation

  • Explore Products

    • Power Modules
    • Discrete MOSFETs
    • Discrete Schottky Diodes
    • Bare Die MOSFETs
    • Bare Die Schottky Diodes
    • Reference Designs
    • Gate Driver Boards
    • Evaluation Kits
    • Materials Products
    • Patents
  • Explore Applications

    • Artificial Intelligence

      • Datacenter & Server Power Supplies
      • Uninterruptible Power Supplies
    • Automotive

      • EV Powertrain
      • On-Board Charger
      • On-Board DC/DC Converter
    • E-Mobility

      • Commercial, Construction & Agriculture Vehicles
      • E-Boats and E-Ships
      • Trains & Traction
    • Industrial Motor Drives

      • Low Voltage Motor Drives
      • Heat Pump & Air Conditioning
      • Servo Drives
    • Renewable Energy

      • Energy Storage Systems
      • Fast Charging
      • Residential & Light Commercial Solar Systems
      • Industrial & Commercial Solar Systems
      • Utility Scale Renewable Energy
    • Materials Applications
  • Tools & Support
  • Explore Company

    • About
    • Locations
    • Senior Leadership
    • Thought Leadership
    • Quality
    • Sustainability
    • News
    • Events
  • Careers
  • Investors
  • English
  • 简体中文 - Chinese (Simplified)
  • 繁體中文 - Chinese (Traditional)
Contact
    View Cart

    Breadcrumb Navigation

    • Home
    • Knowledge Center
    • MOSFETs
    • Silicon Carbide Enables PFC Evolution
    MOSFETs

    Silicon Carbide Enables PFC Evolution

    Aug 17, 2020
    • Share on LinkedIn
    • Share on Facebook
    • Share on Twitter
    • Share in an email

    Article

    Silicon carbide (SiC) power devices have been used in a wide variety of applications, including server power supplies, energy storage systems, and solar-panel power inverters for a long time. The move to electric drive by the automotive industry has recently driven growth in SiC use as well as in design engineer attention toward the benefits of the technology in wider application areas.

    Selecting a device technology

    A shaded graph showing the overlap of GaN, SiC, Si, SJ, IGBT and their performance criteria for Breakdown Voltage Rating.
    Figure 1: These technologies all have their strengths and application areas in which they fit the best.

    No matter what the application, every power supply design starts out by answering the same basic questions: What are voltage in, voltage out, and current out? Next, the designers think about the performance criteria they are trying to enable in their end product. There are a number of technologies at the power supply designer’s disposal today to meet those criteria, including gallium nitride (GaN), SiC, and various silicon (Si)-based technologies like MOSFETs, insulated gate bipolar transistors (IGBTs), and superjunction (SJ) devices (Figure 1).

    When the breakdown voltage rating is below 400 V and the design calls for relatively low-frequency operation at less than a kilowatt, silicon is often a good option. When building a compact application, such as a USB charger, that needs a high switching frequency to reduce the size of the magnetics, GaN is an excellent choice. At power levels over a kilowatt and voltage ratings higher than 600 V and up to about 1,700 V at low frequencies, IGBTs can be considered along with SiC. For higher switching frequency or higher power density, however, SiC is the best.

    Center of choice

    A line graph comparing Wolfspeed's SiC devices against Infineon CoolMOS and GaN systems.
    Figure 2: Wolfspeed’s SiC devices maintain an unchanging low RDS(ON) over a wide temperature range.

    In Figure 1, the moderately high voltages and switching frequencies mark the center of many choices. Yet the high efficiencies offered by SiC make for a compelling option, as weighing BoM cost against operational cost may be a deciding factor.

    The exceptionally low on-resistance of Wolfspeed’s SiC devices means low conduction losses and higher efficiency. Compared with silicon and GaN in this aspect (Figure 2), SiC outperforms all technologies in all applications. The properties of the material itself enable low change in on-resistance over temperatures, whereas RDS(ON) of GaN and silicon increase by 2.5× or more compared with the rating at room temperature.

    Enabling PFC evolution

    Modern rectifiers for power supplies have evolved from the simple bridge rectifiers that required only a “Big Farad Capacitor” to smooth out the DC output. The addition of a passive power factor correction (PFC) stage typically has an LC filter for the line frequency. This works for relatively low-power applications that do not have stringent efficiency and size requirements (Figure 3).

    Flow chart of circuit diagrams showing how to move from a no-PFC design to a basic bridgeless PFC
    Figure 3: The evolution of the full-bridge rectifier from simple no-PFC to basic bridgeless PFC.

    In most switch-mode power supplies today, the boost converter is used after the diode bridge as active PFC that switches several orders of magnitude higher than the line frequency so that smaller inductors and capacitors can be used. Depending on the application, replacing a silicon-based diode with a SiC diode in the active PFC stage can increase efficiency by two to three percentage points.

    On the other hand, increasing the switching frequency from 80 kHz to 200 kHz can reduce the form factor or increase power density by as much as 60%. In general, increasing switching frequency helps reduce the size of the inductor and therefore the copper losses in the inductor as well.

    When going from 200 kHz to 400 kHz, however, a leveling-out of the copper losses is seen while the inductor core losses continue to increase. The result is diminishing returns, where a 10% to 15% reduction in size is accompanied by a 10% to 15% increase in power loss. This may be an acceptable tradeoff for applications in which size reduction is paramount.

    To take the efficiency levels into the higher 90s, the circuit must be redrawn in a way that removes the diode bridge. One way to do this in the boost implementation is to move the inductor to the AC input and swap out the two bottom diodes in the bridge with two MOSFETs. The switch on the left boosts the voltage on the positive half cycle, while the one on the right boosts on the negative half cycle.

    The challenge with the basic bridgeless circuit is that the high-frequency switch node is connected directly to the AC input and the DC ground is floating relative to the AC input. This can cause any parasitic capacitance to go straight into common-mode EMI. A common way around this is to use a dual-boost or semi-bridgeless implementation (Figure 4, left).

    Totem pole topology

    Two circuit diagrams, the left is a Dual-boost Semi-bridegeless solution while the right is a Full-bridge Totem Pole made possible by SiC
    Figure 4: Comparing the dual-boost semi-bridgeless solution (left) with the full-bridge evolution to totem pole topology (right) made possible by SiC.

    An alternative to the dual-boost semi-bridgeless configuration is the totem pole topology that gets its name from the manner in which transistors are stacked on top of each other (Figure 4, right). The totem pole can be built as a full-bridge version, as shown, or as a bridgeless version with the MOSFETs in the low-frequency leg on the right replaced by diodes.

    A line graph showing the reverse-recovery comparison between a SiC and a Si body-diode.
    Figure 5: SiC vs. Si body-diode reverse-recovery comparison.


    The big challenge with totem pole topologies is the reverse-recovery charge of the MOSFET body diode if the converter works in continuous conduction mode (CCM) condition. During the transition from low-side to high-side switches, both FETs cannot be on at the same time, and the body diodes have to conduct during that dead time. The reverse-recovery characteristics of silicon eliminate the efficiency (Figure 5).

    In all hard-switching power supply designs, when the body diode has to conduct, there are reverse-recovery losses. With SiC, which has no minority carriers, there is nearly zero reverse-recovery current. The silicon MOSFET, on the other hand, suffers from several orders of magnitude higher losses. This is what makes silicon unusable in the totem pole.

    For RF power applications that require gigahertz switching speeds at voltages < 50 V and power < 50 W, GaN-on-SiC is the technology of choice. At higher voltages, GaN becomes prohibitively expensive. Moreover, the GaN die size is nearly 3× that of SiC for equivalent current and voltage rating.

    Full-bridge or hybrid totem pole?

    The fully synchronous version of the totem pole is the most efficient implementation. While it can use silicon MOSFETs in the low-frequency leg, only the all-four SiC MOSFET implementation enables bidirectionality — for instance, in applications that connect to a smart grid, with some tradeoff in complexity and BoM cost.

    Most cost-sensitive applications, including server power supplies, use a bridgeless or “hybrid” totem pole topology using inexpensive pin diodes on the low-frequency leg (Figure 6). It has the advantage of using the fewest number of components and, with the introduction of Wolfspeed’s C3M SiC MOSFETs in the 650-V class, it is a cost-effective implementation with less than 0.5% decrease in light load efficiency compared to a full bridge.

    A circuit diagram of a hybrid totem pole. Two parts are circled and labeled to be Wolfspeed's C3M0060065K SiC MOSFET
    Figure 6: A “hybrid” totem pole PFC power stage

    This has already been proved by Wolfspeed’s CRD-02AD065N 2.2-kW reference design that is available for download as a package comprising BoM, schematic, board layout, presentation, and application note. It uses the new 650-V 60-mΩ MOSFETs to achieve the industry standard 80+ Titanium with >98.5% efficiency and THD <5%.

    SiC-based totem pole designs like this significantly exceed the 80+ Titanium requirement under all load conditions, thereby allowing engineers to relax the design constraints on the DC-to-DC converter section.

    To simulate your own design, use the free SpeedFit Design Simulator or get help from application notes, reference designs, and tutorials at Wolfspeed’s Documents, Tools, & Support section online.

    Download File
    Technical SupportPower Applications Forum
    Request SamplesVisit the Sample Center
    SpeedFit Design SimulatorCreate a Design

    Support

    Technical SupportPower Applications Forum
    Request SamplesVisit the Sample Center
    SpeedFit Design SimulatorCreate a Design

    Footer

    Wolfspeed Logo

    Social Media

    • Instagram
    • X
    • LinkedIn
    • YouTube

    Footer Navigation

    • Contact
    • Where to Buy
    • Intellectual Property
    • Suppliers & Contractors

    Legal

    • Privacy Policy
    • Cookie Policy
    • Terms Of Use
    • Accessibility
    Copyright © 2026 Wolfspeed, Inc.

    More Articles

    View All

    Designing with Top Side Cooled (TSC) Silicon Carbide Power Devices 

    Improve thermal management and conserve power with Wolfspeed’s New TSC MOSFETs and Schottky diodes.
    Continue Reading Technical Articles

    Reimagine Auxiliary Power Supply System Durability & Cost with Wolfspeed’s New 1700 V MOSFET Technology

    Continue Reading Technical Articles

    How Wolfspeed Power Modules are Revolutionizing 3-Phase Industrial Low Voltage Motor Drives

    Continue Reading Technical Articles