Wolfspeed Logo

Main menu navigation

  • Explore Products

    • Power Modules
    • Discrete MOSFETs
    • Discrete Schottky Diodes
    • Bare Die MOSFETs
    • Bare Die Schottky Diodes
    • Reference Designs
    • Gate Driver Boards
    • Evaluation Kits
    • Materials Products
  • Explore Applications

    • Artificial Intelligence

      • Datacenter & Server Power Supplies
      • Uninterruptible Power Supplies
    • Automotive

      • EV Powertrain
      • On-Board Charger
      • On-Board DC/DC Converter
    • E-Mobility

      • Commercial, Construction & Agriculture Vehicles
      • E-Boats and E-Ships
      • Trains & Traction
    • Industrial Motor Drives

      • Low Voltage Motor Drives
      • Heat Pump & Air Conditioning
      • Servo Drives
    • Renewable Energy

      • Energy Storage Systems
      • Fast Charging
      • Residential & Light Commercial Solar Systems
      • Industrial & Commercial Solar Systems
      • Utility Scale Renewable Energy
    • Materials Applications
  • Tools & Support
  • Explore Company

    • About
    • Locations
    • Senior Leadership
    • Thought Leadership
    • Quality
    • Sustainability
    • News
    • Events
  • Careers
  • Investors
  • English
  • 简体中文 - Chinese (Simplified)
  • 繁體中文 - Chinese (Traditional)
Contact
    View Cart

    Breadcrumb Navigation

    • Home
    • Knowledge Center
    • OBC & DC/DC Converters
    • Why Choose SiC over Si for Your Next Bidirectional On-Board Charger Design?
    OBC & DC/DC Converters

    Why Choose SiC over Si for Your Next Bidirectional On-Board Charger Design?

    May 12, 2021
    • Share on LinkedIn
    • Share on Facebook
    • Share on Twitter
    • Share in an email

    Article

    Silicon (Si)-based power electronics have long dominated the power electronics industry for their technological maturity and relative ease of accessibility. The silicon carbide (SiC) substrate, however, has gained traction of late due to its major intrinsic advantages, which align well with recent industry trends. This wide-bandgap (WBG) semiconductor can not only handle much larger energy densities than its Si counterpart but also offers a high power conversion efficiency with a large thermal conductivity — factors that are particularly critical in battery-based applications that require a high degree of power savings and fast charges.

    This article is part of a two-part series that discusses the design considerations of on-board charger (OBC) systems and the advantages that SiC has over Si for OBCs, with a focus on bidirectional chargers. The practical advantages of implementing SiC over Si for OBCs are detailed in a comparison of reference designs for a Si and SiC OBC, with a cost savings analysis and breakdown of the system benefits.

    Why SiC?

    SiC has already permeated a myriad of power electronics applications, including power supplies, solar power conversion, power conversion for other renewable energy sources, and inverters for industrial motor drives. This WBG semiconductor is uniquely positioned to serve the bulk of applications on the power spectrum from low-power devices to high-power systems due to its unique combination of critical electric field (2.2 × 106 V/cm), electron velocity, melting point (300°C), and thermal conductivity (4.9 W/cmK). On the transistor level, this leads to a low on-state resistance (R(DS)on) that allows for lower conduction losses, which, in turn, allows for high-current applications. The lower device capacitance relative to Si-based insulated-gate bipolar transistors (IGBTs) enables low switching losses at high switching frequencies with smaller filters, passive components, and an overall simpler thermal management system.

    Table 1 details the benefits of SiC as well as the compounded benefits when leveraging Wolfspeed’s expertise in SiC.

    Table 1

    Wolfspeed Benefit
    Why It Matters
    Highest efficiency (lowest-FOM MOSETs)
    More power delivered to battery = less $$ wasted
    Highest power density
    Saves precious space/weight in the EV and contributes to lower system cost
    System expertise
    Helps accelerate innovation and time to market for customers

    These desirable qualities have catapulted the use of SiC-based AC/DC and DC/DC converters in low-power to high-power electric vehicle (EV) applications. This is particularly true for OBCs that are used in EVs such as e-bikes, hybrid EVs (HEVs), plug-in hybrid EVs (PHEVs), and various battery EVs (BEVs), including commuter cars and commercial trucks. The benefits in doing this include simplifying the charging process and making this technology more palatable for consumers used to the internal combustion engine, or ICE (by mitigating the negative effects of range anxiety).

    For these reasons, charge time and the effective vehicle range after a charge are critical parameters for vehicle manufacturers — two factors that depend upon the battery size and the rated charging power. These charging powers range from lower-power, single-phase systems at 3.3 kW and 6.6 kW to high-power, 11kW and 22kW systems. Figure 1 shows the typical vehicle type, battery size, 0% to 100% charge time, and competitive technologies for 3.3 kw, 6.6 kW, 11 kW and 22 kW OBCs.

    Figure 1: Comparison of vehicle type, battery size, 0% to 100% charge time, and competitive technologies with 6.6-kW and 22-kW OBCs included.
    Figure 1: Comparison of vehicle type, battery size, 0% to 100% charge time, and competitive technologies with 6.6-kW and 22-kW OBCs included.

    Vehicle types range from commuter car BEVs to larger and higher-performance BEVs such as e-trucks. As shown in the image, even with more than 3× the charging power, the larger-capacity vehicles may still have a larger 0% to 100% charge time. This makes OBCs especially efficient for high-power systems; that is, less power is wasted and a quicker charge is obtained.

    Outside of OBC efficiency, parameters such as cost, weight, and size are critical where smaller, lighter OBCs can be more readily implemented in a vehicle, often with a tight space budget. Additionally, OBC cost for both the consumer and for the OEM directly impacts the capex/bottom line of the manufacturer and the ease of accessibility for the consumer. In order to stay competitive, the OBC must help the EV meet the price point of ICE-based vehicles. Use reference designs for 6.6 kW Bi-Directional Totem-Pole PFC and CLLC, optimized for energy efficiency and 6.6 kW Bi-Directional Totem-Pole PFC and CLLC, optimized for power density, to streamline your system design.

    22kW bidirectional OBC designs: Si vs. SiC sample design

    Benefits of bidirectional power flow

    As stated in our earlier unidirectional OBC design piece, bidirectional chargers can inherently achieve higher efficiencies than unidirectional designs due to the omission of the diode losses. The unidirectional DC/DC block includes the use of the Vienna PFC diode, while the unidirectional LLC resonant converter accomplishes output rectification with a diode bridge. Figure 2 shows the typical skeleton of a single-phase bidirectional OBC — the full-bridge rectifier has been replaced with low-loss SiC MOSFETs to eliminate the losses resulting from the forward voltage drop of the rectifier diodes. This, in turn, reduces power dissipation, thereby simplifying thermal management requirements.

    While the Asia-Pacific (APAC) is leading the bidirectional charging initiative for EVs, there is a general trend toward the employment of bidirectional OBCs for their higher system efficiency as well as the potential for V2-other applications, including vehicle-to-home (V2H) power generation, vehicle-to-grid (V2G) opportunities, and vehicle-to-vehicle (V2V) charging use cases (such as jumpstarting another EV).

    Figure 3: Schematic representation of (a) Si-based and (b) SiC-based 22-kW bidirectional OBC.
    Figure 3: Schematic representation of (a) Si-based and (b) SiC-based 22-kW bidirectional OBC.

    22-kW bidirectional OBCs: Si vs. SiC

    As shown previously in Figure 1, Si-based bidirectional OBCs with Si superjunction technologies and Si-based IGBTs are the primary contenders against SiC bidirectional OBCs. However, this section illuminates how SiC exceeds these technologies in all relevant aspects (cost, size, weight, power density, efficiency). Let’s begin by looking at Figure 3, which displays a reference schematic for both a Si- and SiC-based 22-kW bidirectional OBC, showing a side-by-side comparison in the number of power devices and gate drivers.

    Figure 3: Schematic representation of (a) Si-based and (b) SiC-based 22-kW bidirectional OBC.
    Figure 3: Schematic representation of (a) Si-based and (b) SiC-based 22-kW bidirectional OBC.

    Table 2 lists the respective specifications of the first, AC/DC totem-pole PFC stage and the second, DC/DC bidirectional CLLC resonant stages. From both the image and the table, it can be readily seen that there is both over a 30% decrease in power device and gate drivers from the Si design to the SiC design, with the additional benefit of more than double the switching frequency. This leads to a reduced component size, weight, and cost of the power conversion system altogether, all while operating at a greater efficiency. Reference designs for 22 kW Bi-Directional CLLC and 22 kW Bi-Directional Active Front End (AFE) can get you started with bi-directional on-board charger system design.

    Table 2

    22kw Bi-directional OBC: Si vs SiC

    Si-based
    AC/DC Totel Pole PFC Specs
    Vin
    90-277 VAC (1-phase)
    304-504 VAC (3-phase)
    Power Devices
    8 × Si IGBT
    Fs
    20 kHz
    DC/DC Converter Specs
    Vin (DC Link Voltage)
    380-425 V
    Vout
    480-800V
    Power Devices
    16 × 650V Si SJ MOSFET
    Fs
    80-120 kHz
    SiC-based
    AC/DC Totel Pole PFC Specs
    Vin
    90-277 VAC (1-phase)
    304-504 VAC (3-phase)
    Power Devices
    6 × E3M0032120x
    Fs
    45 kHz
    DC/DC Converter Specs
    Vin (DC Link Voltage)
    380-900 V
    Vout
    200-800V
    Power Devices
    8 × E3M0032120x
    Fs
    140-250 kHz

    Cost savings are further broken down in Figure 4 with a system cost breakdown for the Si and SiC systems. The Si system is nearly 20% more than SiC — this is largely due to the comparatively large amount of gate drivers and magnetics in the DC/DC block. So while it can be argued that discrete SiC-based power devices are relatively more expensive than individual Si-based diodes and power transistors, when employed within a system, the capabilities of SiC devices allows for less to be leveraged, therefore cutting down on costs of circuit components required to support the various power device functions.

    Beyond cost savings, the SiC system is able to yield a peak system efficiency of 97% with a power density of 3 kW/L, while the Si OBC accomplishes a 95% efficiency with a power density of only 2 kW/L. This increase in system efficiency could add an annual energy savings of, on average, $40.00 to the consumer.

    Figure 4: System cost breakdown of 22-kW bidirectional OBC in SiC versus Si implementations.
    Figure 4: System cost breakdown of 22-kW bidirectional OBC in SiC versus Si implementations.

    Table 3 compares costs, power density, operational savings, and CO2-based savings between Si and SiC implementations of both a 6.6-kW and 22-kW bidirectional OBC. The savings become much more pronounced the higher up the power spectrum an OBC goes. Both the 6.6-kW and 22-kW bidirectional SiC-based OBCs have a lower BOM cost, ultimately lowering the system cost for the OEM. When combined with the operational savings and the SiC-drive CO2 savings, the savings trickle down to the consumer, thereby closing the price gap with ICE-based solutions while also helping to lower emissions for the planet.

    Table 3: SiC system advantages.

    System Advantage of
    6.6kW bi-direct.
    Si
    SiC
    System cost savings
    enclosure, thermal, magnetics, capacitors
    100%
    98%
    <$5
    Power Density
    OEM-specific $/liter
    >2kW/L
    <3kW/L
    System Efficiency
    (Operational Savings)
    0.55k (0.43)Wh/100km × 30,000km.y × $72/t
    94.5%
    ./.
    97%
    $22/year
    SiC-driven CO2 Savings
    300k km lifetime × 400g/kWH, 0.44 (0.43)kWh/100km × $72/t
    ./.
    $26
    SiC-driven Net Lifetime Savings
    (system cost savings + operational savings + CO2 savings)
    ./.
    ~$355
    System Advantage of
    22kW bi-direct.
    Si
    SiC
    System cost savings
    enclosure, thermal, magnetics, capacitors
    100%
    82%
    >$30
    Power Density
    OEM-specific $/liter
    ca.2kW/L
    ca.3kW/L
    System Efficiency
    (Operational Savings)
    0.55k (0.43)Wh/100km × 30,000km.y × $72/t
    95%
    ./.
    97%
    $32/year
    SiC-driven CO2 Savings
    300k km lifetime × 400g/kWH, 0.44 (0.43)kWh/100km × $72/t
    ./.
    $38
    SiC-driven Net Lifetime Savings
    (system cost savings + operational savings + CO2 savings)
    ./.
    ~$550

    Wolfspeed’s expertise in SiC

    Wolfspeed’s 30-year-plus legacy in the design and development of SiC components and systems helps lower barriers for a designer to employ highly desirable SiC-based components in their next OBC. The combination of Wolfspeed’s broad selection of SiC power devices, SiC systems, and expertise allows for the rapid development of robust design topologies that function reliably in the field. Complete bidirectional OBCs are already available in the Wolfspeed product portfolio along with individual AC/DC and DC/DC stages. This includes a 6.6-kW bidirectional OBC with a 97% system efficiency and 22-kW bidirectional OBC AC/DC and DC/DC converter blocks that can achieve efficiencies as high as 98.6% (Figure 5).

    Figure 5: Wolfspeed’s SiC-based 6.6-kW and 22-kW bidirectional OBC AC/DC and DC/DC blocks.
    Figure 5: Wolfspeed’s SiC-based 6.6-kW and 22-kW bidirectional OBC AC/DC and DC/DC blocks.

    From a full product portfolio to exhaustive engineering and applications support with an online simulation platform and industry experts, Wolfspeed offers a comprehensive foundation for the design and development of SiC systems. This is extended to SiC-based OBCs wherein OEMS can leverage the highly desirable aspects in their next design while cutting on cost, passing the savings from BOM cost and efficiency design down to the customer.

    Support

    Technical SupportPower Applications Forum
    Request SamplesVisit the Sample Center
    SpeedFit Design SimulatorCreate a Design

    Footer

    Wolfspeed Logo

    Social Media

    • Instagram
    • X
    • LinkedIn
    • YouTube

    Footer Navigation

    • Contact
    • Where to Buy
    • Intellectual Property
    • Suppliers & Contractors

    Legal

    • Privacy Policy
    • Cookie Policy
    • Terms Of Use
    • Accessibility
    Copyright © 2026 Wolfspeed, Inc.

    More Articles

    View All

    Engineering for Outcomes:
    Three Ways Wolfspeed Gen 5 Achieves Real-World Performance

    Continue Reading Thought Leadership

    Accelerating Industrial E-mobility 

    More EV users are looking to gain the most of their batteries by leveraging the expanding charging networks around them – either to power their home, a local grid, another vehicle, or receive power from any of these loads via a bi-directional charger. This concept, aptly named Vehicle-to-Everything (V2X), is one way Stercom is enabling more accessible and efficient charging technologies with Wolfspeed Silicon Carbide.
    Continue Reading Case Study

    Gen 4 Silicon Carbide Technology:
    Redefining Performance and Durability in High-Power Applications

    Continue Reading White Paper