• Knowledge Center
    • Powerful Perspectives
    • Beyond Silicon’s Limits: How High‑Voltage Silicon Carbide is Redefining Critical Power
    Powerful Perspectives

    Beyond Silicon’s Limits: How High‑Voltage Silicon Carbide is Redefining Critical Power

    John PerryVice President & General Manager, Medium Voltage & High Voltage Products
    Apr 16, 2026
    • Share on LinkedIn
    • Share on Facebook
    • Share on Twitter
    • Share in an email

    Article

    Global electrification, AI data centers, the energy transition, and critical infrastructure are driving unprecedented power demand — and the loads at the center of this shift are dynamic, bidirectional, and increasingly concentrated at medium- and high-voltage operating points that legacy systems weren't designed to handle. At the infrastructure level, conventional iron-core transformers are passive, uni-directional, physically massive, and too slow to deploy for the pace of modern grid and data center buildout. At the device level, silicon-based semiconductors hit hard physical limits at medium and high voltages — forcing engineers to stack multiple components in series, multiplying losses, heat, complexity, and failure points with every added stage.

    Silicon Carbide changes the equation at both levels simultaneously. SiC's wide bandgap material properties enable dramatically higher breakdown voltages, faster switching speeds, and operation at temperatures where silicon fails — eliminating the need for series-stacked silicon devices and enabling compact, high-efficiency conversion stages across the full MV/HV range. And where iron-core transformers once defined the architecture of power infrastructure, SiC makes possible a new class of Solid-State Transformers that convert medium-voltage grid power directly to usable DC, with bidirectional control, modular form factors, and deployment timelines measured in months rather than years.

    How Mid- to High‑Voltage SiC Changes the Rules

    What’s the solution to power systems at a breaking point? Mid- to high‑voltage silicon carbide (SiC) in power devices that makes previously “unrealistic” architectures viable.

    MV/HV silicon carbide devices offer three fundamental advantages over silicon: 

    • Much higher breakdown voltages, which allow designers to replace long strings of lower‑voltage devices with far fewer high‑voltage switches
    • Higher efficiency and switching frequency, which shrinks magnetics, cooling systems, and overall system footprint
    • High‑temperature capability and robust reliability in harsh environments, which include deep ocean (subsea compressors), far offshore (wind turbines), and deep earth (mining) operations.

    The result is a new set of possibilities across some of the world's most critical and fastest-growing industries:

    • Solid-State Transformers modernizing grid interconnection and data center power delivery
    • HVDC transmission enabling long-distance bulk power delivery, cross-border grid interconnection, and offshore energy integration
    • Utility-scale solar and battery storage inverters operating at 1,500V DC and above
    • Medium-voltage industrial motor drives in heavy industry, mining, and critical manufacturing
    • High-voltage pulsed power systems requiring precise, high-speed switching at gigawatt-scale

    Three Industries Where High‑Voltage SiC is Already Making a Difference

    Let’s look at a few industries where SiC’s unique characteristics rise to the challenge of some of today’s most difficult power realities.

    AI Data Centers: Drastically Reducing Energy Waste and Cooling Costs While Improving Overall System Efficiency.

    High-voltage Silicon Carbide (SiC) is revolutionizing AI data centers by addressing the immense power demands of accelerated computing, offering up to 25–40% reductions in power conversion losses. In addition, SiC's ability to operate efficiently at higher voltages and temperatures reduces the need for massive cooling infrastructure. SiC-based power units can reduce energy costs for cooling by up to 40%, mitigating the high thermal output of GPUs. Using SiC in 11 kW and 25 kW cooling systems can deliver up to 2.4% increases in overall system efficiency.

    Mining and Rare Earths: Turning Energy into Yield

    Traditional mining and mineral processing consume as much as 3-4% of global electricity and approximately 15% of global emissions. Mechanical rock grinding is one of the most energy‑hungry steps. Traditional mechanical spark‑gap switches in pulsed‑power rock crushers wear out frequently, forcing operators to budget for downtime, maintenance, and lost production. High‑voltage SiC enables mining organizations to transition from mechanical grinding systems to pulse-power rock fracturing systems that use ~80% less energy while delivering higher yield. In addition, SiC pulse-power systems offer extremely long operating lifetimes, more precise control, and higher metal recovery per ton of ore, especially important for critical rare earth deposits.

    Subsea Energy and Offshore Wind: Power Where No One Can Service It

    In subsea oil and gas, power electronics sit on the seabed, where a failure can halt production and require costly intervention. Meanwhile, offshore wind turbines are moving to higher voltages and larger blades. Nacelles, the housing that contains all the generating components in a wind turbine, have fixed space but must house ever‑larger converters. Here, high‑voltage SiC converters deliver much higher power density—allowing more power processing capability in the same nacelle footprint—and support 20–25‑year design lifetimes with fewer service visits, reducing the overall cost of energy.

    What’s Held High‑Voltage SiC Back—and Why That’s Changing

    Historic barriers have held full silicon carbide implementation in check. SiC devices are more expensive than commoditized silicon, though simple per‑unit price comparisons ignore system‑level savings. Some standards and qualification for solid‑state transformers and MV/HV SiC in grid equipment remain undefined. And of course, designing safe, reliable 6.5–10 kV gate‑drive and magnetics is non‑trivial and requires highly skilled design engineers with the right tooling.

    But these gaps are closing fast. As adoption ramps in offshore and industrial sectors, costs are falling and supply chains are becoming more robust. Industry collaborations are emerging around standard packages and second‑source strategies to de‑risk supply. And leading SiC innovators are investing in application engineering, reference designs, and validation data to help customers climb the learning curve faster.

    Choosing the Right SiC Partner

    As grid operators, mining operations, and energy companies move beyond incremental silicon upgrades, they will need partners who can provide both devices and deep application expertise. That’s because the shift to high‑voltage SiC isn’t just a technology upgrade; it represents a multi‑decade growth opportunity in mid‑to‑high‑voltage power infrastructure.

    This is where Wolfspeed is playing a central role. Among our own customers, we see how adopting MV/HV SiC is a key driver in building power systems for the next 20–25 years. Wolfspeed’s long history in high‑voltage SiC, work dating back nearly two decades, including development of dozens of devices at blocking voltages up to 27 kV, across many device structures such as MOSFET, IGBT, Thyristor, PiN diodes and JBS diodes. What’s more, our vertically integrated materials‑to‑modules footprint gives us an even further head start on solving the hardest MV/HV problems. This robust experience and expertise enables us to attack MV/HV challenges at every level, from managing crystal growth and thick EPI, to producing SiC materials and devices. We can then translate these achievements into higher performance and better yield on the ground.

    For operators who are designing assets to run flawlessly in deep subsea fields, remote mines, or massive AI data centers, this combination of materials, device, and application expertise is quickly becoming the difference between a promising SiC roadmap and proven, bankable systems in the field. If your MV/HV strategy doesn’t fully leverage what silicon carbide can deliver, it may be time to revisit the assumptions inside your power stack.

    Need Information?Contact Us
    Buy OnlineFind a Distributor

    Support

    Need Information?Contact Us
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
    More Articles

    View All

    Wolfspeed’s 300 mm Silicon Carbide Technology as a Materials Foundation for Next-Generation AI and HPC Advanced Packaging

    Continue Reading  Technical Articles

    Five Qualities to Look for in a Power Electronics Partner

    Continue Reading  Thought Leadership

    The Power of Reclaiming Technology Leadership

    Continue Reading  Thought Leadership